Non-Plug and Play Feedback Devices

To set up a AKD drive with a non-plug and play feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position (for example a resolver or an encoder), you must select a motor from the list of standard or custom motors or enter the motor parameters manually. Once the motor data is entered into KAS IDEClosed"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger, an initial set of parameters can be calculated and downloaded to the drive.

Parameters

The following parameters can be initialized to their default values or calculated from user-supplied motor data:

ILClosed"Instruction list" This is a low-level language and resembles assembly.KP

IL.LIMITN

VL.KP

PL.KI = 0 (Default Value)

IL.KFFACC

IL.LIMITP

VL.KI

PL.INTINMAX = 0.419 (Default Value)

IL.KBUSFF

IL.PWMFREQ

VL.LIMITN

PL.INTOUTMAX = 0.419 (Default Value)

IL.FRICTION

IL.KVFF

VL.LIMITP

MOTOR.IPEAK

IL.OFFSET

IL.FOLDFTHRESHU

VL.THRESH

MOTOR.ICONT

IL.INTEN

IL.FOLDWTHRESH

VL.KVFF

MOTOR.PITCH

IL.IVFB

IL.MFOLDD

PL.KP

MOTOR.POLES

IL.KPDRATIO

IL.MFOLDT

PL.KD = 0 (Default Value)

MOTOR.TYPE

Calculations

KAS IDE uses the following equations to calculate parameter values.

Current Loop

The current loop proportional gain (IL.KP) must be such that the current loop closed loop crossover frequency/bandwidthClosedIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz (BW) nominal is the lesser of 2000 Hz or (PWM Frequency/4).

Then, with this frequency:

IL.KP = 2*π*(desired bandwidth in Hz)*(motor L line-line in H)

Setting the D and Q components

Velocity Loop

VL.KP = (2*π*75)*(2*Jm/Kt) = 300*PI*Jm/Kt

VL.KI = 5

Input - Motor Data

The values for inertia, Jm (Kg / cm2), and torqueClosedTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist constant, Kt (Nm/A), are obtained from either the SFD or the motor model number that you select.

Constants

Velocity Loop BandwidthClosedIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz – BW = The default value is 75Hz.

Input - Inertia Ratio – Q =  The default is 1.

Output - Control Loop Gains

VL.KP = 2 * π * BW * Jm * (1+Q) * 0.0001/Kt

VL.KPI = BW*0.08 -1   (minimum of 1)

PL.KP = BW/5

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen